REC.TRIGTYPE
Description
REC.TRIGTYPE sets the type of trigger.
Input values are as follows:
|
Value |
Description |
|---|---|
|
0 |
Recording starts immediately |
|
1 |
Next command: Recording starts on the next command executed through the TCP/IP. The trigger location in the buffer is set according to REC.TRIGPOS . |
|
2 |
Source signal: Recording starts per the values of REC.TRIGPARAM, REC.TRIGVAL , REC.TRIGSLOPE , and REC.TRIGPOS . |
|
3 |
Boolean: Recording starts when the value of REC.TRIGPARAM is 0 for REC.TRIGSLOPE = 0 or 1 for REC.TRIGSLOPE = 1 |
| 4 | Exact: Recording starts when the value of REC.TRIGPARAM is exactly the value specified REC.TRIGVAL and change happened with REG.TRIGSLOPE slope. |
| 5 | Bitmask: Recording starts when the value of REC.TRIGPARAM masked by REC.TRIGMASK matches REC.TRIGVAL with slope REC.TRIGSLOPE. |
Example
Code
If REC.TRIGPARAM is DIN.STATES and REC.TRIGMASK = 0x3, then the triggering happens only when both DIN1 and DIN2 are high.
-->REC.TRIGTYPE 5
Context
For more information see Scope.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read/Write |
|
Units |
N/A |
|
Range |
0 to 5 |
|
Default Value |
0 |
|
Data Type |
Integer |
|
See Also |
REC.TRIG , REC.TRIGPARAM, REC.TRIGVAL, REC.TRIGSLOPE REC.TRIGPOS |
|
Stored in Non-Volatile Memory |
No |
Variants Supported
All variants are supported.
Fieldbus Information
|
Name |
ID |
Hex |
Data Type |
Access |
Units |
|---|---|---|---|---|---|
|
REC.TRIGTYPE |
2310 |
906 |
Unsigned8 |
Read/Write |
- |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
REC.TRIGTYPE |
2310 |
Unsigned8 |
Read/Write |
- |